- Home
- CRX Prohibit Icon Dragging
In this concise technical walkthrough, we will go over how to enable and manage icon dragging within the timeline editor in a FANUC environment. Guided by Jacob Warczinsky, an application engineer at FANUC America, this session focuses on a practical configuration change that can improve how programs are organized and edited. Whether we are fine-tuning an existing program or building a new one, understanding how to control icon behavior in the timeline can help streamline our workflow and reduce manual effort.
We begin by looking at the default behavior in the timeline editor. While linear points can be added and arranged, icon elements are initially restricted. They cannot be easily removed or reordered by dragging, which can slow down adjustments during development. From there, we will go step by step through accessing the configuration settings that control this functionality. This includes navigating system menus, locating the correct configuration parameter, and toggling the setting that governs icon dragging.
Once the feature is enabled, we will see how icon dragging becomes active directly within the program timeline. This allows us to remove icons by dragging them off the timeline and reposition them as needed. The result is a more flexible editing experience that supports quicker iteration and cleaner program organization. We will also cover how to re-enable the restriction when needed to prevent unintended changes, providing a balance between flexibility and control.
This overview is designed to give you a clear understanding of the process and its benefits without overwhelming you with unnecessary detail. If you are looking to improve efficiency in your programming workflow, this is a valuable feature to understand.
Requirements
- Access to a FANUC system with the timeline editor
- Appropriate permissions to modify system configuration settings
- Familiarity with navigating system and legacy menus
- Basic understanding of program structure in the timeline editor
What you will learn
- How to locate and access configuration settings in the system menu
- Where to find the icon dragging control option
- How to enable icon dragging for program editing
- Methods for deleting and rearranging icons in the timeline
- How to restore the prohibit setting to prevent accidental edits
By the end of this session, we will have a clear path to enabling and managing icon dragging, helping us work more efficiently and confidently within the FANUC timeline editor.
Related Videos
3 - Programming Part 1 - Initial Settings
2 - Unboxing and Setup