5:12
In this video, Senior Engineer Bernhard Walker demonstrates how to set up and use an automatic grid frameset with a connected camera and controller. The process involves navigating to the automatic grid frameset menu, selecting the robot group, user frame or user tool, and camera, and positioning the robot to make the grid visible in the camera's field of view. Adjusting the camera settings and setting the initial start position for the robot are also extremely key steps. The video also covers monitoring the robot's movement, resuming or restarting the process, and successfully setting a user frame or tool frame after completion.