- Home
- Background Logic Timers
In this video, we walk through a practical approach to setting up background logic timers within a robot control environment and explain why this technique can be valuable in real applications. We begin with a relatable scenario involving a gripper system that relies on a vacuum output, where a failure condition requires a controlled retry after a short delay. From there, we explore why traditional methods such as condition monitoring in the main program or using parallel tasks may not always provide the flexibility or reliability needed.
We then move into creating a dedicated background logic program designed specifically for timing behavior. Step by step, we demonstrate how to properly configure the program by removing motion group assignments and preparing it to run independently. As we build this foundation, we also examine common pitfalls, such as attempting to use wait statements in background logic, and why these approaches result in errors.
From that point, we shift into a more effective solution by using registers and scan time to create a timer. By leveraging the controller’s consistent scan cycle, we can increment a register value to simulate elapsed time. We guide you through how to structure this logic, how to calculate timing thresholds, and how to tie those thresholds to specific outputs. Throughout the process, we highlight practical considerations like resetting the timer and preventing register values from growing too large during extended fault conditions.
We wrap up by refining the logic to ensure it runs efficiently in a continuous loop, delivering predictable and repeatable results in a background environment. By the end, we will have a clean, functional solution that can be adapted to a variety of automation needs.
Requirements:
- Basic familiarity with robot programming concepts
- Access to a controller that supports background logic
- Understanding of digital inputs, outputs, and registers
- A defined use case where delayed logic or retry behavior is needed
What You Will Learn:
- How to create and configure a background logic program
- Why wait statements are not supported in background logic
- How to use scan time to build a timer using registers
- How to implement conditional logic based on elapsed time
- Techniques for resetting and managing timer values effectively
- Best practices for maintaining stable and efficient background processes
This overview sets the stage for building more advanced automation logic while keeping your programs organized and responsive.
Related Videos
FANUC Backup and Restore Files
When Should a Robot be used for Machining