- Home
- How to Enable Phase Shift Arc Welding Function
In this video, we will walk through how to enable and verify the Phase Shift function for arc welding, with a specific focus on TIG applications. This feature is part of the Low Frequency Pulse option and is designed for operations that require greater precision and control during wire feed and amperage coordination. Whether we are fine tuning a welding procedure or troubleshooting an existing setup, understanding how Phase Shift works and how to activate it can make a meaningful difference in weld quality and consistency.
We will start by outlining what the Phase Shift function does and why it matters in TIG welding environments. Phase Shift allows us to delay the wire feed command relative to the amperage command, giving more control over how wire is introduced into the molten weld puddle. This added flexibility supports improved wire dabbing behavior and can help stabilize the arc in demanding applications. We will also review the available adjustment range, which spans from negative to positive 180 degrees, and explain how that range affects welding behavior.
Next, we will cover where the Phase Shift function lives within the system and what software versions are required to access it. Since this capability is tied to specific software options and system packages, we will clarify which configurations support it and how to confirm that your system qualifies. From there, we will walk step by step through the process of enabling Phase Shift at cold start using the system menus and variables screen. Once enabled, we will also show how to verify that Phase Shift is active and visible within an individual weld schedule.
This video is designed to give us a clear, practical overview without overwhelming detail, making it easier to follow along and apply the information in real-world situations.
Requirements to use the Phase Shift function include:
- Core software version V8.30P/01 or newer
- J584 Low Frequency Pulse option
- R799 Heatwave Sync or J582 TIG Arc Weld Package
In this video, we will learn how to:
- Understand the purpose and benefits of the Phase Shift function
- Identify compatible software versions and required options
- Enable Phase Shift through the system variables menu
- Verify that Phase Shift is active within a weld schedule
If we are looking to expand control over TIG welding performance and gain deeper insight into advanced system features, this video provides a strong foundation and clear next steps.
Related Videos
Overview of Adaptive Welding with a 3rd Party Sensor
How to turn on Adaptive Welding for R-50iA